Post Go back to editing

10/19/17 Which tampering features can be detected that a neutral current measurement cannot ensure?

Which tampering features can be detected that a neutral current measurement cannot ensure?

  • On behalf of David Lath.
    Simply monitoring the neutral helps increase the number of tampers caught, but using mSure increases the number even further. The example shown in the webinar of a double bypass tamper is which  cannot be caught by monitoring the neutral because both line and neutral are bypassed and therefore no difference is measured with a live-neutral comparison.