Post Go back to editing

ADN2820 Question

Dear Sir/Madame

      I would like to use your TIA ADN2820 with an photo-diode. The functional block diagram proposed in Figure 1. of datasheet has the anode of photo-detector connected with input pin (IN). However, I have only access to cathode of our photo-detector and the anode is directly connected to ground. Can be this request satisfied using your TIA ADN2820, having the photo-diode correctly biased and respecting all the chip specifications? If not, may Analog propose other TIA?

Yours sincerely, Carlos Ferreira 

Parents
  • Dear Carlos,

    What is the max. data rate you target to support upto?

    Could you share me your selected photo-diode datasheet for a review?

    Which ROSA package you would like to bond this TIA and your photo-diode to, butterfly or TO-46, for example?

    In general, ADN2820 supports common cathode photo-diodes.

    However, the TIA IN pin voltage is clamped by an internal +0.85V. So, if this is a good reverse bias voltage

    to your photo-diode, you are welcome to try your common anode photo diode. Of course, when do this,

    you can not copy Fig. 1 circuitry directly.

    Best Regards,

    Dongfeng

Reply
  • Dear Carlos,

    What is the max. data rate you target to support upto?

    Could you share me your selected photo-diode datasheet for a review?

    Which ROSA package you would like to bond this TIA and your photo-diode to, butterfly or TO-46, for example?

    In general, ADN2820 supports common cathode photo-diodes.

    However, the TIA IN pin voltage is clamped by an internal +0.85V. So, if this is a good reverse bias voltage

    to your photo-diode, you are welcome to try your common anode photo diode. Of course, when do this,

    you can not copy Fig. 1 circuitry directly.

    Best Regards,

    Dongfeng

Children
No Data