Post Go back to editing

AD8232 output wrong ECG chart with no R wave, and it always srop down to 0

Category: Hardware
Product Number: AD8232
Software Version: Arduino IDE 2.1.0

I used AD8232 and esp32 to design an ECG monitor system, however came through the problem that the output is obviously wrong, it didn't hace a R wave and T wave, and I also wondering that if it's wrong that the output always drop down to 0?

For hardware connection. I used Power supply generator for AD8232 module, and choose esp32-s for the microcontrollor.

The code is as follow:

#include <PubSubClient.h>

/****************************************
 * Include Libraries
 ****************************************/
#include <WiFi.h>
#include <PubSubClient.h>

#define WIFISSID "NUSRI-STU"                         // Put your Wifi SSID here
#define PASSWORD "Nusri311"                          // Put your WIFI password here
#define TOKEN "BBFF-qfd0nIe1xM2AVibTAxTigxq2ViA2i3"  // Put your Ubidots' TOKEN
#define MQTT_CLIENT_NAME "e7ja5ddcxff"               // MQTT client Name, please enter your own 8-12 alphanumeric character ASCII string;
                                                     //it should be a random and unique ascii string and different from all other devices

/****************************************
 * Define Constants
 ****************************************/
#define VARIABLE_LABEL "sensor"  // Assign the variable label
#define DEVICE_LABEL "esp32"     // Assig the device label

#define SENSOR A0  // Set the A0 as SENSOR

char mqttBroker[] = "industrial.api.ubidots.com";
char payload[100];
char topic[150];
// Space to store values to send
char str_sensor[10];

/****************************************
 * Auxiliar Functions
 ****************************************/
WiFiClient ubidots;
PubSubClient client(ubidots);

void callback(char* topic, byte* payload, unsigned int length) {
  char p[length + 1];
  memcpy(p, payload, length);
  p[length] = NULL;
  Serial.write(payload, length);
  Serial.println(topic);
}

void reconnect() {
  // Loop until we're reconnected
  while (!client.connected()) {
    Serial.println("Attempting MQTT connection...");

    // Attemp to connect
    if (client.connect(MQTT_CLIENT_NAME, TOKEN, "")) {
      Serial.println("Connected");
    } else {
      Serial.print("Failed, rc=");
      Serial.print(client.state());
      Serial.println(" try again in 2 seconds");
      // Wait 2 seconds before retrying
      delay(2000);
    }
  }
}

/****************************************
 * Main Functions
 ****************************************/
void setup() {
  Serial.begin(115200);
  WiFi.begin(WIFISSID, PASSWORD);
  // Assign the pin as INPUT
  pinMode(SENSOR, INPUT);

  Serial.println();
  Serial.print("Waiting for WiFi...");

  while (WiFi.status() != WL_CONNECTED) {
    Serial.print(".");
    delay(500);
  }

  Serial.println("");
  Serial.println("WiFi Connected");
  Serial.println("IP address: ");
  Serial.println(WiFi.localIP());
  client.setServer(mqttBroker, 1883);
  client.setCallback(callback);
}

void loop() {
  if (!client.connected()) {
    reconnect();
  }

  sprintf(topic, "%s%s", "/v1.6/devices/", DEVICE_LABEL);
  sprintf(payload, "%s", "");                    // Cleans the payload
  sprintf(payload, "{\"%s\":", VARIABLE_LABEL);  // Adds the variable label

  float sensor = analogRead(SENSOR);

  /* 4 is minimum width, 2 is precision; float value is copied onto str_sensor*/
  dtostrf(sensor, 4, 2, str_sensor);

  sprintf(payload, "%s {\"value\": %s}}", payload, str_sensor);  // Adds the value
  Serial.println("Publishing data to Ubidots Cloud");
  client.publish(topic, payload);
  client.loop();
  delay(500);
}

Sinserely hoping for an answer.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.