MAX17330
Not Recommended for New Designs
The MAX17330 is not recommended for new designs. The replacement part is the MAX17332.
The MAX17330 is a 28μA IQ stand-alone charger, fuel gauge, protector...
Datasheet
MAX17330 on Analog.com
The charge current can be configured using an appropriate sense resistor. For example, a 500mOhm sense resistor can be used to set the charge current to a very small value of 10mA needed for tiny cells in the range of 10mAhr. On the other hand, a 2mOhm sense resistor can be used to get 5A needed for fast-charging 5Ahr batteries.
The charge current can be configured using an appropriate sense resistor. For example, a 500mOhm sense resistor can be used to set the charge current to a very small value of 10mA needed for tiny cells in the range of 10mAhr. On the other hand, a 2mOhm sense resistor can be used to get 5A needed for fast-charging 5Ahr batteries.