Post Go back to editing

Overall Gain of the receiver from T/R module till ADC output

Hi,

As per demo platform what is the overall coherent gain acheived  till ADC output in the receive mode including the stingray board, x band up down converter and ad9081 board.

Could you please tell the availability of the 5 watt and 10 watt T/R module i.e. the next higher version of adtr1107

Parents
  • Hi akladha, 

    I'll point you to some data that you can use in your own cascade analysis. There are a few sets of data: ADXUD1A, ADAR1000EVAL1Z, and the EVAL-AD9081 datasheet. There are additional components in the signal path that may or may not be included in your final design listed on the X-Band Development Platform product page under System Requirements (e.g. splitter/combiner, cables, etc.).

    Single channel RX gain at 10 GHz for the RF section is approximately 31 dB whereas the RX full scale input (including the ADCs where full scale input is +6 dBm) is -25 dBm with a -50 dBm input power. These values are calculated/measured for a signal chain including the ADAR1000EVAL1Z ->  ZX10-2-183-S+ Mini Circuits Splitter/Combiner -> ADXUD1AEBZ -> 4 inch RF Cable -> EVAL-AD9081. Coherent combining would result in a cumulative gain of 49 dB for the RF section and RX full scale input of -43 dBm. In this design there are 4 subarrays where each subarray consist of 8 channels for a total of 32 coherently combined channels (20log10(8) signal gain improvement and 10log10(4) noise improvement). 

    Regarding the 5W/10W TR modules, I spoke too soon mentioning these parts in the webinar recording. They are still early development and it's too early to determine availability. Apologies for the misdirection.

    Regards, 
    Sam 

Reply
  • Hi akladha, 

    I'll point you to some data that you can use in your own cascade analysis. There are a few sets of data: ADXUD1A, ADAR1000EVAL1Z, and the EVAL-AD9081 datasheet. There are additional components in the signal path that may or may not be included in your final design listed on the X-Band Development Platform product page under System Requirements (e.g. splitter/combiner, cables, etc.).

    Single channel RX gain at 10 GHz for the RF section is approximately 31 dB whereas the RX full scale input (including the ADCs where full scale input is +6 dBm) is -25 dBm with a -50 dBm input power. These values are calculated/measured for a signal chain including the ADAR1000EVAL1Z ->  ZX10-2-183-S+ Mini Circuits Splitter/Combiner -> ADXUD1AEBZ -> 4 inch RF Cable -> EVAL-AD9081. Coherent combining would result in a cumulative gain of 49 dB for the RF section and RX full scale input of -43 dBm. In this design there are 4 subarrays where each subarray consist of 8 channels for a total of 32 coherently combined channels (20log10(8) signal gain improvement and 10log10(4) noise improvement). 

    Regarding the 5W/10W TR modules, I spoke too soon mentioning these parts in the webinar recording. They are still early development and it's too early to determine availability. Apologies for the misdirection.

    Regards, 
    Sam 

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.