Post Go back to editing

What is the best available performacne, assuming I can support some increase in current consumption?

Thread Summary

The user inquired about the performance of the ADXL367 accelerometer at low power consumption. The final answer confirmed that the ADXL367 operates with less than 2μA current over a supply range of 1.1 to 3.6V, providing up to 400 samples per second (SPS) and noise levels 300 times lower than the force of gravity (3.1 mg).
AI Generated Content
Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.