KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
MAX77540
Recommended for New Designs
The MAX77540 is a high-efficiency step-down converter
with two 3A switching phases. It uses an adaptive COT
(constant on-time) current-mode control architecture...
Datasheet
MAX77540 on Analog.com
MAX77540 is available in ADI's FCQFN package. This package however does not support the I2C interface and as such limits the capablity and programmability of the device.
Is there a 3D STEP file available for the 22 pin FC2QFN (4.25x4.25) package