Post Go back to editing

What parts are included in the system kit?

  • The ADAR1000EVAL1Z, ADXUD1AEBZ, AD-9081 EVAL, and all necessary power supplies and control cables are provided in the kit. Reference/Example MATLAB software is also provided. All design files (schematic, BOM, layout) are provided upon purchase of the kit. Users will need to separately procure the Xilinx ZCU102 Development board, 2:1 Power Splitters, and RF cabling to connect all channels. Also, the 10 GHz lattice spaced planar antenna tiles are provided upon request when purchasing the ADAR1000EVAL1Z.