KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
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
A single sensor can cover up to 5m in radius, where the radius is the maximum distance from center to corner in a rectangular room (approx. 50 sqm). Height is 8 to 12 feet (2.4 to 3.65m) and field of view with the fisheye lens is 180 degrees.
A single sensor can cover up to 5m in radius, where the radius is the maximum distance from center to corner in a rectangular room (approx. 50 sqm). Height is 8 to 12 feet (2.4 to 3.65m) and field of view with the fisheye lens is 180 degrees.