Post Go back to editing

Do mSure reports put an extra burden on AMI networks?

mSure reports are fairly small. It’s a 64-byte packet for one-phase meters and 128 bytes for 3-phase meters. They don’t need to be sent as often as the electricity consumption data. We provide the flexibility for a DSO or the meter company supporting the DSO to adjust the period of which the mSure reports are sent over the AMI network. It could be hourly, daily, or less frequent. It has very little impact on the bandwidth because the reports are very small.

  • Answer: mSure reports are fairly small. It’s a 64-byte packet for one-phase meters and 128 bytes for 3-phase meters. They don’t need to be sent as often as the electricity consumption data. We provide the flexibility for a DSO or the meter company supporting the DSO to adjust the period of which the mSure reports are sent over the AMI network. It could be hourly, daily, or less frequent. It has very little impact on the bandwidth because the reports are very small.