Post Go back to editing

Question for LTC3309A application

I have used LTC3309A from 5Vin to 3.3Vout, Frequency:2MHz(With RT connecting to Vin for Default value), and Vout  setting for 3.3V; Sync/Mode is tied to Vin for Burst mode.

Question/Problem: I find the output voltage is dropped with the load is rised, ez: output current 0A, vout:3.3V; ouput current 1A, vout:3.25V; output current 3A, vout: 3.18V; output current 6A,

vout:3.1V.  This problem will cause my FPGA core voltage not steady and may make my FPGA broken down. Would someone help me to handle this case. Thanks.

Parents Reply
  • Dear Marty:

    I have done some tests on my board.

    I'll find the FB voltage dropped(FB voltage will drop to 0.47V while the output current is about 6A) while the load becomes heavier. 

    I have reviewed the Datasheet and find the LTC3309A is the 1st generation Silent Switch technology architecture. So the Caps should place symmetrical with Vin and Vout. 

    In the meanwhile, the LTC3309A on my board can't startup with Heavy load. And due to the SS pin may be design inside the IC, so I can't change the SS cap to set the startup current.

    Could you please give me some advice?

Children