Does the LT8614 come multiple output channels? Is there micromodule option with LT8614?
Does the LT8614 come multiple output channels? Is there micromodule option with LT8614?
On behalf of Anthony Armstrong:
The LT8614 is a Single Output step-down converter which can deliver up to 4A of continuous output current. We currently have four 42V input capable dual output devices: the LT8653S with dual 2A per channel, the LT8650S with dual 4A per channel, the LT8650SP with dual 7A per channel and the LT8616 with dual 2.5A & 1.5A per channel device. The micromodule regulator that uses the LT8614 inside of it is the LTM8024.