Post Go back to editing

Why should we use dedicated cabling for cameras when there are royalty free codecs?

Why should we use dedicated cabling for cameras when there are royalty free codecs, such as AV1 which use low bandwidth over CAT5e cable?

Parents
  • On behalf of Fionn Hurley:
    Automotive has very specific requirements especially around EMI/EMC performance. Cable thickness and weight are also a major factor for automotive. Latency is also a key requirement for automotive and therefore heavier compression solutions are to be avoided. Even for Ethernet connectivity in the vehicle new standards were developed and did not consider CAT5e cables as a viable option and instead also went with UTP cabling. Given all of these using AV1 codec with CAT5e does not look like a viable solution for automotive. 

Reply
  • On behalf of Fionn Hurley:
    Automotive has very specific requirements especially around EMI/EMC performance. Cable thickness and weight are also a major factor for automotive. Latency is also a key requirement for automotive and therefore heavier compression solutions are to be avoided. Even for Ethernet connectivity in the vehicle new standards were developed and did not consider CAT5e cables as a viable option and instead also went with UTP cabling. Given all of these using AV1 codec with CAT5e does not look like a viable solution for automotive. 

Children
No Data