What will be the Physical connectivity between C2B Tx to C2B Rx? Eg: 2 wire or 4 wire? What will the supported baud rate in C2B?
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
What will be the Physical connectivity between C2B Tx to C2B Rx? Eg: 2 wire or 4 wire? What will the supported baud rate in C2B?
On behalf of Fionn Hurley:
The C2B video data and bi-directional control channel run over a single twisted pair (two wire) link. In some applications power will be provided from the Rx side of the link and this would require and additional two wires (Power and Ground). The link runs up to maxim link clock speed of 150MHz.