A single sensor can cover up to 5m in radius, where the radius is the maximum distance from center to corner in a rectangular room (approx. 50 sqm). Height is 8 to 12 feet (2.4 to 3.65m) and field of view…
A single sensor can cover up to 5m in radius, where the radius is the maximum distance from center to corner in a rectangular room (approx. 50 sqm). Height is 8 to 12 feet (2.4 to 3.65m) and field of view with the fisheye lens is 180 degrees.