Post Go back to editing

Is the ADuM4166 USB 2.0 compliant?

Parents Reply
  • The 'test modes' ConalW refers to are the 'hi speed' testmodes defined in USB 2.0 chapter 7.1.20.  ADuM3165/3166/4165/4166 do not fully support detection of the commands to enter these modes, or the actual entry.  However, the products include alternate test capability enabling checking of all items normally tested with the USB 2.0 chapter 7.1.20 hi speed test modes.  Analog Devices has performed these alternate tests and confirmed passing results. 

Children
No Data