About the Webcast

Today's vehicles are becoming more and more quiet, which in return has made the customer highly sensitive to acoustical comfort! Thus, the "my car is making a funny noise..." scenario is a major challenge for system architects and designers. On one hand, it needs to be ensured that no disturbing noise is heard and on the other hand, the perceived sound quality needs to fulfill the listener's expectations with respect to the sound design. Through this webcast we will explore new automotive applications for acoustic processing and the signal processing technologies that enable them.

  • Advanced voice processing technologies enabling new applications such as personal audio zones (PAZ) and in-car communication (ICC) will be explored
  • We will also discuss the relevance of techniques such as adaptive noise control (ANC) and road noise cancellation (RNC) to these applications and others 
  • Finally, we will present the  technologies and solutions that ADI can offer to address the challenges associated with implementing these new applications

Download the presentation here.

Related Links:

ADI's A2B Solution Solves the Audio Design Challenges of Tomorrow

Analog Devices: Acoustic Echo Cancellation Algorithm (AEC)

Highly Deterministic Real-Time Audio Processing with the ADSP-2156x SHARC Product Family

Answered Questions
There are no posts to show. This could be because there are no posts in this forum or due to a filter.
Open Questions