About the Webcast

To realize the goals of Industry 4.0, highly connected, intelligent and flexible manufacturing, new industrial connectivity solutions are required that enable higher data bandwidth and deliver a converged network between the IT and OT. With the increased deployment of robots and cobots in new smart factories, significantly more data is being generated and distributed along with real time control commands. This is creating the need for enhanced Gigabit real-time Ethernet communications with Time Sensitive Networking capability. As the process industry embraces Industry 4.0, sensors/actuators require Ethernet connectivity on single twisted pair cabling up to a distance 1km (new IEEE standard 802.3cg-2019 / 10BASE-T1L) in intrinsically safe, Zone 0 applications. This presentation discusses the challenges and solutions of new Ethernet technologies for tomorrow’s Industrial communications systems. 

  • Learn about how to deploy an industrial Ethernet Solutions today for 10/100Mbit,
  • Understand what TSN is, why is it needed and where is it headed.
  • Learn about the future of edge connectivity with 10BASE-T1L

Download the presentation here.

Related Links:

Find out about ADI's leading products, solutions and software offerings.

Read more on the trends at play within Industrial Connectivity and how that is accelerating the transition to Industry 4.0

Learn more about Ethernet to the edge with 10BASE-T1L

Answered Questions
Open Questions
There are no posts to show. This could be because there are no posts in this forum or due to a filter.