• 12/13/18 Silent Switcher Regulators: High Efficiency with Ultralow EMI

    12/13/18 Silent Switcher Regulators: High Efficiency with Ultralow EMI

    A switching regulator is typically the first active component on the input power bus line and therefore has a significant impact on the EMI performance of the complete circuit. There are two types of EMI emissions...
    Jan 3, 2019   92831 members
  • 11/29/18 Knocking Down the Barrier to Autonomous Driving

    11/29/18 Knocking Down the Barrier to Autonomous Driving

    The future is upon us. Vehicles are getting more capable in the area of autonomy, yet there are still significant hurdles to overcome to realize safe and ubiquitous autonomous transport. This Webcast will discuss...
    92831 members
  • 11/08/2018 Six Cybersecurity Must-Haves to Secure the Edge

    11/08/2018 Six Cybersecurity Must-Haves to Secure the Edge

    The world is going digital. To participate, we have to connect and trust data being generated and exchanged. What does trust mean? How is trust the foundation of a "resilient" connected system? How is trust established...
    92831 members
  • 10/31/18 Automotive Camera Connectivity using C2B Technology

    10/31/18 Automotive Camera Connectivity using C2B Technology

    In this webcast we will discuss automotive camera connectivity. We will cover OEM pain points, key requirements and different technology solutions. We will also introduce Analog Devices Car Camera Video Bus (C2B). C2B is a new automotive camera link techno
    Apr 23, 2020   92831 members
  • 10/11/18 The Four Pillars of Optimizing Analog Integration

    10/11/18 The Four Pillars of Optimizing Analog Integration

    Without a doubt, analog and mixed signal designs are hard. When selecting an integration path, the one with the most value is the one that not only solves the most challenging problems but simplifies the entire design.
    Nov 11, 2019   92831 members
  • 09/27/18 RF Technology for 5G mmWave Radios

    09/27/18 RF Technology for 5G mmWave Radios

    In this webcast, we discuss the various technologies that may be applied to mmWave beamforming systems for 5G base stations. We start with an overview of the use cases, which in turn influence the radio architectures that best suit the deployment case.
    92831 members
  • 7/19/18 The Evolving Requirements of Smoke Detection

    7/19/18 The Evolving Requirements of Smoke Detection

    This webcast reviews the critical requirements of smoke detectors and how and why those requirements are evolving. We discuss the major types of detectors and their advantages / disadvantages
    Apr 24, 2019   92832 members
  • 7/26/18 The Hidden Cost of Your Isolated System Design

    7/26/18 The Hidden Cost of Your Isolated System Design

    Market and technology trends are driving increased complexity in isolated system design. Changes in electromagnetic compatibility and safety certification requirements create risk and drive up development costs. Learn about new solutions for isolated power
    92832 members
  • 6/28/18 Design Challenges for Aerospace and Defense SDR

    6/28/18 Design Challenges for Aerospace and Defense SDR

    This webcast will provide an overview of design challenges faced by next generation aerospace and defense software defined radio (SDR) platforms. These platforms often need higher channel counts, improved performance, smaller size, and lower power. At the
    92832 members
  • 6/7/2018 Industry 4.0 - Industrial Ethernet and the Transition to Time Sensitive Networking

    6/7/2018 Industry 4.0 - Industrial Ethernet and the Transition to Time Sensitive Networking

    Industrial Ethernet has now been in the market for nearly 20 years and is the preferred communication technology in industrial automation. However, with the standardization of Time Sensitive Networking (TSN) and the drive towards the convergence of IT and
    92832 members
  • 5/17/2018 Technologies for Wearable and Clinical Vital Signs Monitoring

    5/17/2018 Technologies for Wearable and Clinical Vital Signs Monitoring

    Vital Signs Monitoring (VSM) can be found in a broad range of markets and use cases, and each of them have their challenges and key requirements. Analog Devices is providing technologies to address these applications and markets. In this webcast you will l
    May 21, 2018   92832 members
  • 5/3/2018 Making Precision Signal Chain Design Easier

    5/3/2018 Making Precision Signal Chain Design Easier

    n this webcast, we'll take a look at some key areas where Precision signal chain development can be simplified for the designer. First, we'll look at what a design engineer should take into a consideration at the component level, focused on convert
    92832 members
  • 4/5/18 Enabling Next-Generation EW and Phased-Array Systems

    4/5/18 Enabling Next-Generation EW and Phased-Array Systems

    Enabling Next-Generation EW and Phased-Array Systems 2018 web
    92832 members
  • 4/19/18 - Simplify Power Designs with Micromodule Products

    4/19/18 - Simplify Power Designs with Micromodule Products

    This webcast explains our µModule (micromodule) DC/DC power products. They are complete system-in-package (SiP) power management solutions with integrated DC/DC controller, power transistors, input and output capacitors, compensation components and inducto
    Sep 21, 2020   92832 members
  • 3/6/2018 Streamlining Flexible System Design using RF ADCs with DSP

    3/6/2018 Streamlining Flexible System Design using RF ADCs with DSP

    Highly integrated and versatile RF ADCs support a large variety of system designs with their DSP feature sets. This webcast explores how these devices ease the system design complexities of today's radio architectures. A typical customer’s design cycl
    Nov 11, 2019   92832 members
  • 3/22/18 Best PCB Layout Practices for Frequency Synthesizers

    3/22/18 Best PCB Layout Practices for Frequency Synthesizers

    This webcast is an overview of the best techniques for the optimal layout of Frequency Synthesizers, with a particular emphasis on Phase Locked Loops (PLLs).
    92832 members
  • 2/27/18 JESD204B Link Debugging Guidelines

    2/27/18 JESD204B Link Debugging Guidelines

    JESD204B provides fewer interconnects which simplifies layout and allows smaller form factor realization without impacting overall system performance. This webcast begins with general JESD204B link debugging guidelines, regardless of product. We then go de
    Jul 1, 2021   92832 members
  • 2/15/18 Innovative Isolated RS-485, SPI and LVDS Communications

    2/15/18 Innovative Isolated RS-485, SPI and LVDS Communications

    This webcast shows the benefits of Analog Devices' combined interface and isolation portfolio for several application examples including RS-485 solutions for Military, Aerospace and Industrial applications requiring high EMC immunity; isolating SPI int
    92832 members