Does the LT8614 come multiple output channels? Is there micromodule option with LT8614?

Does the LT8614 come multiple output channels? Is there micromodule option with LT8614?

  • On behalf of Anthony Armstrong: 
    The LT8614 is a Single Output step-down converter which can deliver up to 4A of continuous output current. We currently have four 42V input capable dual output devices: the LT8653S with dual 2A per channel, the LT8650S with dual 4A per channel, the LT8650SP with dual 7A per channel and the LT8616 with dual 2.5A & 1.5A per channel device. The micromodule regulator that uses the LT8614 inside of it is the LTM8024.