Do you have any examples with maximum distance achieved for the isolated LVDS with the ADN4651?

Do you have any examples with maximum distance achieved for the isolated LVDS with the ADN4651?

Parents
  • 0
    •  Analog Employees 
    on Feb 16, 2018 8:06 PM

    On behalf of Richard Anslow:

    Typically you can use the ADN4651 with less than 10 meter cable lengths.

     

    The cable length that you can use with the ADN4651 will depend on:

    • The cable quality and specification
    • The jitter requirements for your application
    • The LVDS receiver specification at the far end of the cable
    • The LVDS data rate used, for example 200 Mbps, 300 Mbps …
Reply
  • 0
    •  Analog Employees 
    on Feb 16, 2018 8:06 PM

    On behalf of Richard Anslow:

    Typically you can use the ADN4651 with less than 10 meter cable lengths.

     

    The cable length that you can use with the ADN4651 will depend on:

    • The cable quality and specification
    • The jitter requirements for your application
    • The LVDS receiver specification at the far end of the cable
    • The LVDS data rate used, for example 200 Mbps, 300 Mbps …
Children
No Data