With the various technologies being considered, do you see InP being a significant player perhaps after the initial rollout?

With the various technologies being considered, do you see InP being a significant player perhaps after the initial rollout?

  • 0
    •  Analog Employees 
    on Mar 27, 2017 11:16 PM

    Answered on behalf of Dr. Thomas Cameron.

    In the frequency range up to 80GHz, I haven’t seen any requirement to date for InP. As far as I know InP is more expensive than Si or GaAs based technologies. However, as the industry progresses up into the terahertz range, InP may very well be a required technology.