Questions about HMC1121

Hello,
 I am working in a design and looking for a PA with 5.1 - 5.9 GHZ  frequency range .
The HMC1121 PA looks great but I have several questions about this part:1.- Frequency range is 5.5 - 8.5 GHZ but  plots on page 8 show the behaviour from 4 - 5 GHZ to 9 GHZ. Could I have a problem if this part is used from 5.1 GHZ to 5.9 GHz?2.- In the absolute maximum ratings table, the thermal resistance (Rth) is 4.4 ºC/W. is that right?. I am asking that because in a similar packages I saw greater thermal resistance.3.- About the same maximum rates table: there is not limitations on maximum and/or minimun voltage for Vgg on this table. How could I get those values?
Regards,
  • 0
    •  Analog Employees 
    on Mar 22, 2018 11:27 PM

    Hi,

    1. I don't see there is a problem using it from 5 - 6 GHz range as there is good performance there.

    2.  Depending on the die, the thermal resistance can vary even if they are using the same package.

    3. I would recommend to keep the min and max for Vgg between -2 to 0V.

    Best Regards,

    David