Hi.I've connected the AD5761 For the programming of the AD5761, I did the following steps:- write to control_reg <= X"0400DE";// output range =0 to 15VI load the input dac register with X"ffffff" data to get 15V on VoutThe Vout is always 0V, the signals seem to me correct.
what is the problem
I have used erite and update register, now it's working. Thanks
Hello,
I also use this ad5761R,and i can readback the register correctly,but the Vref=0.75,not the 2.5V, i think the schematic is not correct,can you share your schematic ?
thanky you very much!