i'am looking for a 16bits DAC microcontroler compatible with a spi or i2c interface

I'm making a stall generator using a D/A Converter and a pic microcontroller.
i need a DAC wich uses a 10v reference, and it's output is a voltage rate of (0 to 5v, or 0 to 10v )

i went the portfolio my self but i got lost in all those choices, and the ones i found good for my application didn't use a 10v reference or a had a SOIC package and not PDIP.

Parents
  • 0
    •  Analog Employees 
    on Apr 4, 2018 12:11 PM

    Hi,

    Can you explain more what a stall generator is doing?

    If you only want to generate an output ranges of 0V-5V and 0V-10V, then you can just use AD5683R which can output 0-2.5V and 0-5V (for a reference of 2.5V), then just an amplifier at the output with a gain of 2.

    Cheers,

    Ivan

Reply
  • 0
    •  Analog Employees 
    on Apr 4, 2018 12:11 PM

    Hi,

    Can you explain more what a stall generator is doing?

    If you only want to generate an output ranges of 0V-5V and 0V-10V, then you can just use AD5683R which can output 0-2.5V and 0-5V (for a reference of 2.5V), then just an amplifier at the output with a gain of 2.

    Cheers,

    Ivan

Children
No Data