Post Go back to editing

REF192 dropout

Hi,

I need some more information on REF192 dropout at current output < 1 mA.

In the documentation it is indicated that with a current of 10 mA, the dropout is 1v.

Is it possible to have an idea of the dropout witha current of 500 µA ?

In our application, the REF192 will have a power supply input of 3.3v and we want to be sure that it will output the correct voltage reference of 2.5v.

Thanks for your answer

  • Hi Nadir,

    I see in the table on the datasheet that the value you are pointing to is a maximum dropout voltage value at 3.3V Vs.

    I'm looking at the datasheet right now, and on page 19 figure 19, there is a graph of dropout voltage vs load current, and at 10 mA, the typical dropout voltage is only at 0.3V.  If you look at 1mA (2 times what your asking about) it looks like 0.06V  So I would expect that type of performance. (it says REF195, but this is for the REF19x family)

    I'm going to move this to the voltage reference community to see if they have any further comments.

    Regards,

    Brandon

  • NA,

      Fig 19 is for the REF195, which is similar to the REF192.  If you look at fig. 20 in the d.s.,

    the pass element is a PNP, so Vce(sat) is probably less than 0.3V, so you should not have

    any problem.  However, why use the REF192, which is more than 20 years old?

    Look at the ADR3425 spec table which has specs a lot closer to what you need, and it's

    three years old and 30% cheaper.

    Harry

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.