Post Go back to editing

ADR421 VIN Range

Hi, 

For the ADR421 device, what is the minimum voltage for the VIN input? 

In our design, we are planning to use it for the  VIN=5V and VOUT=2.5V.

However, our input voltage may degrade and becomes between the 4.75V and 4.925V. For the voltage VIN=4.85V, does output voltage also degrade? What will be the output voltage for such a case? Does the output voltage stay in range [2.475V, 2.525V] ? 

Thanks in advance.

Top Replies

  • Hi  the specified voltage range for ADR421 is from 4.5V to 18V so the output will stay on the range of what is specified on the datasheet. 

    A Grade: 2.497 to 2.503

    B Grade: 2.499 to 2.501

    Best regards…

Parents Reply Children
No Data