Post Go back to editing

Problem to make the LT6650 work as adjustable negative shunt reference

Thread Summary

The user encountered issues replicating a -1.65V output from an LT6650 negative reference on a breadboard, achieving only -893mV. The final solution involved adjusting R1 to 68kΩ to achieve -2.21V and settling on R3 at 47kΩ, resulting in a stable -2.187V output. The support engineer suggested considering a negative LDO like the LT3093 for better stability, but the user required a stable reference over temperature, making the LT6650 a suitable choice.
AI Generated Content
Category: Hardware
Product Number: LT6650

Hello,

I try to use the LT6650 as a negative reference to get around -1,65V at the output. I draw a simulation that work perfectly but I cannot make it works when I assemble all the components on a breadboard. What I get is -893mV on the output.

I would like to understand why it did not work and how to make it work.

Please find in attached file the schematics and simulation files that I try to replicate.

Regards,

NMaquet

LT6650-negative.asc

  • Hi, R3 is requiring nearly all the current that LT6650 can sink and it needs it for startup. I recommend setting R3 to 100k. In addition C2 should be larger per the datasheet. 

  • Hello BrendanWhelan,

    Thank you very much for your answer. I tried 100k but the circuit worked even worse.
    We have some load on Vout (around 22k) and It seems to interact with the circuit.
    I finally change the value of R1 to  68K to have -2.21V and then I tried different values for R3 and settled again on 47K. A measure -2.187V which is acceptable for my use case.
    I feel like there is something missing to get the values of resistors with a load on the component.

    Regards,

    NMaquet

  • Yes, that would completely change the circuit, as it is balancing the current. Is the load on Vout connected to Ground? Or -12V. You need to account for the current in the load relative to the current in R3. Is the load constant? If not, the circuit will not work. I suspect you would have better luck with a negative LDO product.

  • Hello BrendanWhelan,

    Thank you for your answer. The load is connected to the output of another LT6650 that generate positive voltage. I took into account the current in R3 and add it to the formula in the datasheet. Now I think we have a stable circuit.
    We cannot use negative LDO in our use case because we need a stable reference and LDO is not stable enought regarding temperature.

    Best regards,

    NMaquet

  • I'm glad you found a solution. We do have some very stable LDOs such as LT3042 (and LT3093 for negative voltages) which are about 2% accurate over temp.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.