Post Go back to editing

Voltage noise density curve

Thread Summary

The user requested a voltage noise density curve from 1Hz to 100kHz. The final answer indicates that the curve is not available, but the 1kHz noise can be considered flat-band, intersecting with 1/f noise below 1kHz and extending to around 10kHz. The flatband noise is dominant, as shown in the time-domain plot with a 100x scale compared to low-frequency noise.
AI Generated Content
Category: Hardware
Product Number: ADR03

I am looking for a voltage noise density curve (for frequency from 1Hz to 100kHz) instead of the 1 point value available on the datasheet. 

If the curve is not available values at each point from 1 to 100kHz will be usefull too. 

Thanks 

Best regards 

  • We don't have that curve available. It is generally fair to assume that the 1kHz noise is flat-band, so it intersects with 1/f noise somewhere below 1kHz and runs out to the BW of the internal buffer, likely around 10kHz. You can reasonably look at flatband noise as dominant as the time-domain plot shows a scale of 100x vs. the low-frequency noise.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.