The example of a programmable current source (06526-023) in the ADR5040/1/3/5 datasheet (ADR5040/ADR5041/ADR5043/ADR5044/ADR5045 (Rev. E)) appears to be misconnected. The op-amps inverting input is used as the feedback pin on the drain of the mosfet, but this pins voltage has an inverse relationship to the op-amps output voltage. The stronger the amp drives the transistor, the more current will flow and therefore the lower the voltage on the feedback pin will drop. In the currently pictured config, the FET will never turn on, and if it did, it would be saturated immediately.
The feedback should be on the non-inverting pin, so that when the signal voltage is given to the inverting pin, the amp will attempt to drive it up to VDD, turning the FET on and dropping the feedback voltage instead.