Post Go back to editing

Why is the output voltage of the ADR3650A outside the expected range?

Category: Hardware
Product Number: ADR3650

Hello,

I'm using an ADR3650ARMZ voltage reference with a 20-bit ADC (AD4020BRMZ). We have noticed an issue with some ADR3650A units after power-up. Occasionally, the output voltage (5V) of the ADR3650A does not fall within the specified range (Datasheet +/-0.08% => 4.996 to 5.004 V). In fact, most of the time we measure 4.999V, but occasionally, on start-up with certain ICs, the reference voltage stabilizes at a voltage > 5 V + 0.08% (for example 5.013 V or 5.021 V => 0.42%). This problem occurs in around 10% of chips (always the same identified). And unfortunately, it's not always easy to reproduce the problem.

The input voltage of the ADR3650 is +5.8V and is generated by an LT3045. The output voltage is connected to:

  • a op-amp follower connected to the ADC Vref pin
  • a 2x10k resistive divider with an op-amp follower to provide a Vref/2 voltage
  • 100nF and 1μF

The difference in Vref output voltage is causing a major problem for our ADC conversion of the measurement signal between system power-ups.

Do you have any idea what might explain this behavior of the ADR3650A?

The LT3045 currently has a soft start of around 700ms. Could it be that the Vref doesn’t like slow voltage rises?

Are we drawing insufficient current from the output (currently 0.25mA)?  I haven’t seen any minimum requirement in the datasheet.

The dropout voltage is 0.8V. It's more than the minimum 0.3V (in 10mA specification). Am I right?

Could a poor soldering profile have damaged some of the ICs?

If you have any suggestions, please let me know.

Thank you

Sebastien

Parents
  • Hi Sebastien,

    We don't have specifications for the ADR3650 rise time, but generally 700ms is on the very long side of startup times for references.

    Did you see the frequency of incorrect voltages change at all with the 44ms rise time? And given the fast-startup function has seemed to address the issue (let us know otherwise), what specifically did you change--just the two feedback resistors from PGFB to OUT?

  • Hi,
    I can’t say whether, with a rise time reduced to 44 ms, the frequency of Vref failures is as high as it is at 620 ms. I haven’t carried out that test. I experienced it three or four times during the test, and even once is unacceptable in our application. However, with a rise time of 12 ms, I haven’t yet been able to reproduce the problem. It looks very promising so far...
    And yes, I’ve only implemented the ‘RPG’ resistors between the Vout and PGFB pins of the LT3045 to enable the fast start-up function up to 90% of Vout.

Reply
  • Hi,
    I can’t say whether, with a rise time reduced to 44 ms, the frequency of Vref failures is as high as it is at 620 ms. I haven’t carried out that test. I experienced it three or four times during the test, and even once is unacceptable in our application. However, with a rise time of 12 ms, I haven’t yet been able to reproduce the problem. It looks very promising so far...
    And yes, I’ve only implemented the ‘RPG’ resistors between the Vout and PGFB pins of the LT3045 to enable the fast start-up function up to 90% of Vout.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.