Post Go back to editing

Design Inquiry

Thread Summary

The user is inquiring about the start-up time for the ADR4525BRZ voltage reference when used with the DAC AD3552R. The support engineer suggests it should be a few tens of microseconds, similar to the ADR444. The input capacitors are 0.1uF and 1uF, and the output capacitors are two 1uF and one 0.1uF.
AI Generated Content
Category: Hardware
Product Number: ADR4525BRZ, ADR4525

Hi Team,

I'm planning to use ADR4525BRZ as 2.5V voltage reference for the DAC AD3552R

What is the start-up  time for the IC as i couldn't get those details in datasheet.

The Cin capacitors provided are 0.1uF and 1uF

The Cout capacitors provided are two 1uF and one 0.1uF

Regards,

Abhishek

Parents Reply Children
No Data