Post Go back to editing

Design Inquiry

Thread Summary

The user is inquiring about the start-up time for the ADR4525BRZ voltage reference when used with the DAC AD3552R. The support engineer suggests it should be a few tens of microseconds, similar to the ADR444. The input capacitors are 0.1uF and 1uF, and the output capacitors are two 1uF and one 0.1uF.
AI Generated Content
Category: Hardware
Product Number: ADR4525BRZ, ADR4525

Hi Team,

I'm planning to use ADR4525BRZ as 2.5V voltage reference for the DAC AD3552R

What is the start-up  time for the IC as i couldn't get those details in datasheet.

The Cin capacitors provided are 0.1uF and 1uF

The Cout capacitors provided are two 1uF and one 0.1uF

Regards,

Abhishek

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.