Post Go back to editing

MAX6035

Thread Summary

The user questions the inconsistency in the MAX6035 datasheet where Vin is listed as 5V, but the dropout voltage is ~2V. The final answer clarifies that most tests are conducted with Vin = 15V, and dropout testing is done with Vin = Vout + 1.9V.
AI Generated Content
Category: Datasheet/Specs
Product Number: MAX6035

MAX6035 datasheet for 5V output version, top of the 2 tables (pages 4 & 5) states Vin=5V.  But Dropout voltage is ~2V.

What should Vin be at the top of the table (since Vin=5V is incorrect)?

Graphs show Vin=15V.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.