Post Go back to editing

Output voltage changes in relation to ambient temperature for the MAX6102

Thread Summary

The user inquired about output voltage fluctuations in the MAX6102 due to ambient humidity changes, specifically at 1% RH and 85% RH. The final answer stated that this data is not available for the MAX6102 but suggested referring to the ADR45505 datasheet's HUMIDITY SENSITIVITY section for related information.
AI Generated Content
Category: Datasheet/Specs
Product Number: MAX6102

Hello.

I have questions about MAX6102.

Is there any data on output voltage fluctuations caused by fluctuations in ambient humidity for the MAX6102?
The two types of data I would like to see are as follows.

① Output voltage at low humidity (1% RH)
② Output voltage at high humidity (85% RH)

Best regards.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.