Hello,
I'm looking into using the ADR3650 as the excitation source and voltage reference in a data acquisition application with a bridge sensor (e.g. a mV/V load cell). My basic design is to use the ADR3650 to power the load cell, an AD8557 instrumentation amplifier an ADC and DAC, and also be the VREF input to the ADC and DAC in the system. This way everything will be ratiometric from the ADR3650 and I only need a single supply for the analog end of the system. My board design is 4-layers and I'm looking at using a copper pour area on one of the planes to handle the output from the ADR3650 to feed the other devices rather than running traces. However, I have some concerns:
- The ADR3650 seems like a relatively new chip (which I like), but it is not yet in wide distribution - so my team has some supply concerns. What can ADI say about availability of the chip?
- Related to #1, I don't see much in the way of design guides, blog posts etc. for the ADR3650 chip in terms of practical layout examples, etc. Any practical design layouts available from ADI besides what I see for the Eval module? Or is it pretty much standard to treat the ADR3650 as a voltage reference / LDO?
- What do you think of using the copper pour for the ADR3650 output, and if OK, will it matter how I connect the power and ground planes back to the Vout (Force/Sense) and GND (Force/Sense) pins on the device?
- Am I asking too much of the ADR3650 to do all this? Would it be better to use a separate LDO to power the ADC and DAC and use the ADR3650 only as the reference for these devices? I can see using the ADR3650 to power the load cell and the AD8557, while providing the REF voltage to the ADC and DAC to keep the measurement chain ratiometric. But since the ADC and DAC need only <1mA for power each, I thought the ADR3650 could handle that load as well with no issue.
Thanks in advance for your help and inputs!
-Dino