Post Go back to editing

adr1001 BUF_F pin

Category: Hardware
Product Number: adr1001

I saw the "SHORT-CIRCUIT CURRENT LIMIT" in the datasheet of ADR1001. Could anyone tell its detailed meaning to me? 

Moreover, is it safe to short the BUF_F pin to GND or VCC? In other words, can the BUF_F pin be connected to GND or VCC through a small resistor (for example,10mΩ) for a short period (about 10 seconds) without causing permanent damage?  (For example,when using it as a calibration source, accidentally shorting two connectors.)

More specifically, when the op amp output is shorted to the ground or source, the op amp will still work because the short-circuit protection. And its current is given in the "SHORT-CIRCUIT CURRENT" of the datasheet. Some op amps can even be shorted for long time. However, in the ADR1001 datasheet, I found that it has an extra "LIMIT", which caused me confused.

Edit Notes

correct a mistake
[edited by: MRT17 at 8:22 PM (GMT -5) on 12 Dec 2024]