Post Go back to editing

REF02AZ/883C

Good morning. My name is Jose Maria Diaz, I belong to the Quality Department of the company MADES SA, located in Malaga, Spain.
We have a question regarding a device we have purchased (REF02AZ/883C). The material purchased is DC: 2231 and we have proceeded to compare it against unds we have in stock from our factory (DC: 1527).in the test we have done, the unds of our stock, we have verified continuity between GND pin and NC pins (1,7,8).in the unds in stock, the measurements made (ohm), gives us open circuit, but in the unds received, the measurement between pin 4 and 8 / 1, gives us a value of 23 Kohm approx. and between pin 4 and 7 of 400 ohm. approx.
Which has made us suspect the device.
Can you tell us if the device is correct? it is perhaps a modification in the design (there are 7 years of difference between the two DC).
What other tests could we perform for verification?
Waiting for your answer, best regards.

Thread Notes