Post Go back to editing

MAX6126A25+ maximum output capacitance

Category: Hardware
Product Number: MAX6126A25+, MAX6126

Hello,

we are using MAX6126A25+ to create voltage reference for two ADCs AD4695BCPZ.

We successfully implemented the following scenario on our prototypes:

- single 0.1uF cap on MAX6126A25+ OUT(F) pin

- two 10uF caps on each ADCs AD4695BCPZ REF pin

Still, we would like to make sure that we are within the spec for the maximum output capacitance of MAX6126A25+ voltage reference but this information is not available in the datasheet.

Any suggestions?

Best regards,
Dusan