Does the MAX6241 have an LTSPice model? Regards.
MAX6241
Production
The MAX6225/MAX6241/MAX6250 are low-noise, precision voltage references with extremely low 1ppm/°C temperature coefficients and excellent ±0.02% initial...
Datasheet
MAX6241 on Analog.com
Does the MAX6241 have an LTSPice model? Regards.
We do not yet have LTspice models for the MAX voltage references. We are working on that, so keep your LTspice updated.
Are there some information when it will be released (more or less)? I would like to use it for a simulation too. It would make some things easier.
Hello,
Currently the only MAX reference is the MAX6037_ADJ - could this potentially be useful to you regarding simulation?
Regards,
Jeff
Thank you! I will try it.