Post Go back to editing

Hickup with 10 uF at ADR130 output

Category: Hardware
Product Number: ADR130
Software Version: NA

Hello,

in a design with minimal resistive  load on the ADR130 0.5 Volt output, but with 10 u capacitor, two ADR130 I tested mostly stayed at 0V output. By repeated switching on and off power, sometimes nominal 0.5 Volt output was reached. Changing the 10 u to 0.1 u output capacitor made the part work as expected. In AR130 datasheet D I see no hint on unexpected behaviour with a large output capacitor. ADR130 input voltage is provided by ADP151-3.3, with 10u at the input and 10 Ohm to ADP151. Please consider documenting that behaviour.

Best regards

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.