I have to change from the ADR130 to a possible replacement ADR510 because the ADR130 hast about 2 years for delivery .
I have stacked two ADR130 to generate a 1.0V and a 2.0V reference for my TMS320F2812.
Can i stack the ADR510 as well ?
KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
ADR510
Production
Designed for space critical applications, the ADR510 is a low voltage (1.000 V), precision shunt-mode voltage reference in an ultracompact (3 mm × 3 mm...
Datasheet
ADR510 on Analog.com
ADR130
Production
The ADR130 is the first family of tiny, micropower, low voltage, high precision voltage references in the industry. Featuring
0.35% initial accuracy and...
Datasheet
ADR130 on Analog.com
I have to change from the ADR130 to a possible replacement ADR510 because the ADR130 hast about 2 years for delivery .
I have stacked two ADR130 to generate a 1.0V and a 2.0V reference for my TMS320F2812.
Can i stack the ADR510 as well ?
Hi adr510
Can you share the specs that you need? There may be another product that may be a better fit.
After looking at the data sheet, it seems reasonable that ADR510 could be stacked. I will order some parts to see if this works since stacking is not mentioned on the applications section.
Best regards,
Gio
Hi adr510
Can you share the specs that you need? There may be another product that may be a better fit.
After looking at the data sheet, it seems reasonable that ADR510 could be stacked. I will order some parts to see if this works since stacking is not mentioned on the applications section.
Best regards,
Gio
Hello Gio,
i have tried it myself and it is possible to stack them. I need these two voltages for an TI TMS320F2812.
Thanks a lot