Post Go back to editing

Ask a question about ADR440

Category: Hardware
Product Number: ADR440
Software Version: None

Hi,

Now, I want to ask a question about ADR440. As below, this is the specification in the datasheet. If the input voltage is less than 3V, such as 2.548V(2.048V+0.5V), is the output voltage 2.048V ?

If the input voltage is less than 2.548V, what about the output voltage? Will it be less than 2.048V?

Thanks!