Post Go back to editing

EVAL-AD5791SDZ ,EV-LTZ1000-REFZ

i want to design motherboard for the EV-LTZ1000-REFZ,  SO i need the .brd of the board or gerber files to know the accurate distance between the connectors and the pins. where i can find this information? files of EVAL-AD5791SDZ can also being useful for me.

i already see the information in the EVAL-AD5791SDZ , there is layout but i can export from there the distances because its not the same scale as the real board.

sahar



extra information
[edited by: sahar37 at 10:42 AM (GMT -4) on 18 Aug 2021]
  • Hi Sahar,

    Please use the list below

    UUNITS = MILLIMETERS

    J4    7.5000      30.0000   90 m    CNTHFHDR1X3L300W100H165
    J5    77.5000    45.0000   90 m    CNTHFHDR1X3L300W100H165
    J6    20.0000    7.5000    180 m   CNTHFHDR1X3L300W100H165
    J9    77.5000    30.0000   90 m    CNTHMHDR1X3L300W100H284
    J1    7.5000      15.0000   90 m    CNTHMHDR1X3L300W100H284
    J2    40.0000    47.5000   180 m  CNTHMHDR1X3L300W100H284
    J3    20.0000    47.5000   180 m  CNTHMHDR1X3L300W100H284
    J7    40.0000    7.5000     180 m  CNTHMHDR1X3L300W100H284
    J8    77.5000    15.0000   90 m    CNTHMHDR1X3L300W100H284

    Regards,

    Mon