Post Go back to editing

Stacking the ADR504x.

Hi,

Examples of stacking circuit has been posted on the ADR5045 data sheet.
Please refer to Figure.21.

Figure 21a shows three ADR5045 devices configured to give 15 V.

 

Examples of Stacking circuit has been posted on the ADR5045 data sheet.
Please refer to Figure.21.

Is it possible with reference to the figure, to generate a -0.5V using the ADR5043 (3.0V) and ADR5041 (2.5V)?

Amplifier because it causes the noise, but they do not consider it used.
Is it possible to configure only voltage reference?