Hello
One of my customer is considering ADR06.
The capacitive load would be 4uF. Can ADR06 drive it?
Should they use buffer amplifier?
If you have advice, it is helpful.
Regards,
Shumpei
ADR06
Production
The ADR01, ADR02, ADR03, and ADR06 are precision 10.0 V, 5.0 V, 2.5 V, and 3.0 V, respectively, band gap voltage references featuring high accuracy...
Datasheet
ADR06 on Analog.com
Hello
One of my customer is considering ADR06.
The capacitive load would be 4uF. Can ADR06 drive it?
Should they use buffer amplifier?
If you have advice, it is helpful.
Regards,
Shumpei
I found the comment up to 10uF would be OK for Cout.
Hi Shumpei,
Yes, that should be fine. It is actually recommended on its datasheet to put an additional 1 uF to 10 uF electrolytic, tantalum or ceramic capacitor at the output to improve transient performance response to sudden changes in load current.
Let me know if you need anything else.
Best regards,
Emman