KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
REF192
Production
The REF19x series precision band gap voltage references use a patented temperature drift curvature correction circuit and laser trimming of highly stable...
Datasheet
REF192 on Analog.com
AD8138
Production
The AD8138 is a major advancement over op amps for
differential signal processing. The AD8138 can be used as a
single-ended-to-differential amplifier or...
Datasheet
AD8138 on Analog.com
REF191
Production
The REF19x series precision band gap voltage references use a patented temperature drift curvature correction circuit and laser trimming of highly stable...
Datasheet
REF191 on Analog.com
Hi, i'm Jeong Ho Lee from vpixmedical
Firstly, i appreciate to your help about last question of potentiometer.
It really helps!
Anyway, I have a question about REF19x series.
We try to use REF19x as a kind of reference(?) voltage at -IN pin of AD8138. (See schematic below)

When input signal(PMT signal) of +IN pin of AD8138 above 2.5 V, because of feedback loop of AD8138, i think current will flow from '-IN' pin of AD8138 to 'Out' pin of REF192.
That means sink current occur to REF192.
We do experiment of the output of REF 192 but there's no change of REF192 output while input signal change 0 V to 5 V.

It works but, we really concern about that is either abnormal or not.(I can't find data of how much sink current REF19x series can take)
Question
1. How much sink current REF192 can take?
2. Is it okay to change REF192 to REF191 on above schematic?
Thank you
Hi Jeong Ho Lee,
The REF192 is not tested to sink current. Sinking current using this might/might not cause problem for the device. It is not guaranteed by the datasheet. To be sure for the product to work, I recommend using a sinking resistor.
For the second question, I think there is no problem in Voltage Reference side. It's just a question of does changing your voltage from 2.5V to 2.048V applicable in your application.
Regards,
Mon
Hi Jeong Ho Lee,
The REF192 is not tested to sink current. Sinking current using this might/might not cause problem for the device. It is not guaranteed by the datasheet. To be sure for the product to work, I recommend using a sinking resistor.
For the second question, I think there is no problem in Voltage Reference side. It's just a question of does changing your voltage from 2.5V to 2.048V applicable in your application.
Regards,
Mon