Post Go back to editing

AD588ARWZ alternatives

Hello,

I have seen on the Analog website that the AD588 is not recommended for new designs. Is there a one on one alternative available that is recommended for new designs?

Kind regards, Jonas

Parents
  • Hi Jonas,

    Could you give me more information on what application, supposedly, you are going to use the AD588?

    Do you have a specific specs that you are aiming to use?

    Thanks,

    Mon

  • Hi Mon,

    I'm already using the AD588 in a current design.  The AD588 is used as the control element of a bipolar bridge in combination with an AD620 to amplify the output value of the bridge. The reason I asked if the are any one-on-one alternatives (same pinout and package and with the same or better specs concerning drift, error, etc...) is because I wanted to know if I could change my bill of materials to another chip without the need of changing my pcb design when the AD588 becomes obsolete.

    Kind regards, Jonas

Reply
  • Hi Mon,

    I'm already using the AD588 in a current design.  The AD588 is used as the control element of a bipolar bridge in combination with an AD620 to amplify the output value of the bridge. The reason I asked if the are any one-on-one alternatives (same pinout and package and with the same or better specs concerning drift, error, etc...) is because I wanted to know if I could change my bill of materials to another chip without the need of changing my pcb design when the AD588 becomes obsolete.

    Kind regards, Jonas

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.