Post Go back to editing

Absolute Maximum rating ADR291/2

Thread Summary

The user inquired about the absolute maximum rating of the Vout pin, especially in cases where Vin is less than Vout. The support engineer provided curve trace graphs showing the internal circuit trips at around 0.5V difference between Vout and other pins, recommending Vout-Vin < 0.5V. The engineer also suggested adding external ESD protection if needed.
AI Generated Content

Hi , 

could you please let me know the Absolutist Maximum rating of  Vout pin .

I would like to know this because there are case when the input falls below the Vout and  Vin < Vout (Capacitor).

Thanking you 

With best regards and wishes 

Parents Reply
  • Hi Kabekami

    I tried to do some Curve Trace see graph below:

    1. Vout vs GND

    2. Vout vs Vin

    As you can see the internal circuit will trip at around .5V difference between the Vout and the other 2 pins. With this I would recommend to keep the Vout-Vin<0.5V. I'm still not sure if these response is that of the ESD or other else. 

    If need be, please add some external ESD that will trip below the trip point shown above at the output pin.

    Best Regards,

    Mon

Children
No Data