Hi ,
could you please let me know the Absolutist Maximum rating of Vout pin .
I would like to know this because there are case when the input falls below the Vout and Vin < Vout (Capacitor).
Thanking you
With best regards and wishes
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADR291
Production
The ADR291 and ADR292 are low noise, micropower precision voltage references that use an XFET® reference circuit. The new XFET architecture offers significant...
Datasheet
ADR291 on Analog.com
Hi ,
could you please let me know the Absolutist Maximum rating of Vout pin .
I would like to know this because there are case when the input falls below the Vout and Vin < Vout (Capacitor).
Thanking you
With best regards and wishes
Hi Kabekami,
I'm looking in to this. I'll get back to you once I get the data.
Best Regards,
Mon
Hi Kabekami
I tried to do some Curve Trace see graph below:
1. Vout vs GND

2. Vout vs Vin

As you can see the internal circuit will trip at around .5V difference between the Vout and the other 2 pins. With this I would recommend to keep the Vout-Vin<0.5V. I'm still not sure if these response is that of the ESD or other else.
If need be, please add some external ESD that will trip below the trip point shown above at the output pin.
Best Regards,
Mon